The TMWriteFile API call writes the file specified by the file handle 'file_handle' with the data from the buffer 'write_buffer', containing 'num_write' bytes. 'file_handle' must be set as a result of a call to TMCreateFile. This API call works only with regular files with extensions 0-99 decimal and the ‘Monetary File’ with extension 101. For ‘add’ files with extension 100 decimal, use the API call TMWriteAddFile. In case of the ‘Monetary File’, multiple retries will NOT be attempted. If the file was written many times, then the counter would not end up where it was expected. If this function fails then the file must be closed and then recreated with TMCreateFile. If the Counter has changed then the file needs to be re-encrypted.
For a description of the above types, see the TMEX Type Descriptions.
Parameters
session_handle
Specifies the session handle returned from the API function TMExtendedStartSession that specifies the desired 1-Wire network port. This parameter is required by most TMEX API functions.
state_buffer
Specifies a pointer to a memory location that TMEX keeps all of the state information for the 1-Wire networks. This parameter is required by most TMEX API functions.
file_handle
Specifies a file handle of the file to read.
write_buffer
Specifies a pointer to a buffer that contains the data to write to the file. It must be at least ‘num_write’ bytes long.
num_write
Specifies the number of bytes to write from the ‘write_buffer’.
Return Value
>= 0 => file written, and this is the number of bytesSee Also