The TMTouchReset API call performs the Reset function on the 1-Wire network, resetting all of the devices on the 1-Wire network. The function returns the result of the operation.
For a description of the above types, see the TMEX Type Descriptions.
Parameters
session_handle
Specifies the session handle returned from the API function TMExtendedStartSession that specifies the desired 1-Wire network port. This parameter is required by most TMEX API functions.
Return Value
0 => No presence pulse detected.See Also