Session
TMExtendedStartSession request a 1-Wire network port
TMStartSession (old format) request a 1-Wire network port
TMValidSession check to see if the 1-Wire network port session is still valid
TMEndSession relinquish a 1-Wire network port
File Operations
TMFirstFile get first file name in the current directory
TMNextFile get next file name in the current directory
TMOpenFile open a file for reading
TMCreateFile create a file for writing
TMCloseFile close an opened/created file
TMReadFile read an opened file
TMWriteFile write a created file
TMDeleteFile delete a file
TMFormat format 1-Wire device for file structure
TMAttribute change file/directory attributes
TMReNameFile rename a file
TMChangeDirectory read or change the current directory
TMDirectoryMR Make or Remove a sub-directory
TMCreateProgramJob ready the write buffer for EPROM programming
TMDoProgramJob do the EPROM programming
TMWriteAddFile append or alter an ‘AddFile’ on an EPROM 1-Wire device
TMTerminateAddFile terminate an ‘AddFile’ with Universal Data Packets
TMGetFamilySpec gets 1-Wire device description based on family code
Get_Version read the version string of the main TMEX driver
Transport
TMReadPacket read a CRC16 validated packet
TMWritePacket write a CRC16 validated packet
TMBlockIO transfer a block to the 1-Wire network
TMExtendedReadPage read a device-CRC validated page (regular or status)
TMProgramByte program a byte in an EPROM 1-Wire device
TMProgramBlock program a block of bytes in an EPROM 1-Wire device
TMCRC provides 8-bit or 16-bit CRC calculation
Network
TMFirst find the first device on a 1-Wire network
TMNext find the next device on a 1-Wire network
TMAccess select the current device
TMStrongAccess verify that the current device is still there and select
TMStrongAlarmAccess same as TMStrongAccess except it must be alarming
TMOverAccess select the current device and switch it into overdrive speed
TMRom read the current device ROM or set the ROM for the next select
TMFirstAlarm find the first alarming device on a 1-Wire network
TMNextAlarm find the next alarming device on a 1-Wire network
TMFamilySearchSetup set the search to find a family type on the next search
TMSkipFamily skip the current device family type on the next search
TMAutoOverDrive automatically get in and out of overdrive speeds
TMSearch performs general search for 1-Wire devices
Hardware Specific
TMSetup verify the port exists
TMTouchByte one byte communication to 1-Wire network
TMTouchReset reset 1-Wire devices on 1-Wire network
TMTouchBit one bit communication to 1-Wire network
TMProgramPulse send a programming pulse to 1-Wire network
TMOneWireLevel set the 1-Wire communication level
TMOneWireCom set the 1-Wire communication speed
TMClose power down a port (not always applicable)
TMGetTypeVersion read the version string of the hardware specific driver
TMBlockStream transfer a stream to the 1-Wire network
TMReadDefaultPort reads the default 1-Wire port and type from the system registry
TMGetAdapterSpec returns 1-Wire adapter feature-set information
See Also
TMEX API Overview, TMEX API Alphabetized Function List