TMEX Hardware Specific API Overview Overview Group

The TMEX Hardware Specific API layer functions described in this section are provided to enable the lowest level of communication to 1-Wire devices. With the exception of TMSetup and TMClose, these API calls should not need to be called when using normal file-oriented TMEX operations. The more complex levels of TMEX call this layer for all operations.

See Also

TMEX Hardware Specific API List, TMEX Hardware Specific Error Return Codes