TMExtendedReadPage Code Example

long session_handle;
unsigned char state_buffer[15360], read_buffer[100];
short len;

/* session_handle set from a call to TMExtendedStartSession */
...

/* the internal 8-byte ROM buffer contains a valid ROM that is going to be selected to do a device specific operation */
...

/* attempt to read page 0 of the status memory */
len = TMExtendedReadPage(session_handle, state_buffer, 0, read_buffer, 1); 

if (len >= 0)
{
   /* success, status page read and its length is len */
   ...
}
else
{
   /* TRANSPORT error reading extended page (did this device have 
      extended read?) */
   ...
}

/* close the session with a call to TMEndSession */
...