com.dalsemi.onewire
Class OneWireAccessProvider

java.lang.Object
  |
  +--com.dalsemi.onewire.OneWireAccessProvider

public class OneWireAccessProvider
extends Object

The OneWireAccessProvider class manages the Dallas Semiconductor adapter class derivatives of DSPortAdapter. An enumeration of all available adapters can be accessed through the member function EnumerateAllAdapters. This enables an application to be adapter independent. There are also facilities to get a system appropriate default adapter/port combination.

Usage

Example 1

Get an instance of the default 1-Wire adapter. The adapter will be ready to use if no exceptions are thrown.
 
  try
  {   
     DSPortAdapter adapter = OneWireAccessProvider.getDefaultAdapter();
        
     System.out.println("Adapter: " + adapter.getAdapterName() + " Port: " + adapter.getPortName());
     
     // use the adapter ...

  }   
  catch(Exception e)
  {
     System.out.println("Default adapter not present: " + e);
  }
  

Example 2

Enumerate through the available adapters and ports.
 
  DSPortAdapter adapter;
  String        port;

  // get the adapters
  for (Enumeration adapter_enum = OneWireAccessProvider.enumerateAllAdapters();
                                  adapter_enum.hasMoreElements(); )
  {
     // cast the enum as a DSPortAdapter
     adapter = ( DSPortAdapter ) adapter_enum.nextElement();

     System.out.print("Adapter: " + adapter.getAdapterName() + " with ports: ");

     // get the ports
     for (Enumeration port_enum = adapter.getPortNames();
             port_enum.hasMoreElements(); )
     {
        // cast the enum as a String
        port = ( String ) port_enum.nextElement();

        System.out.print(port + " ");
     }

     System.out.println();
  }
  

Example 3

Display the default adapter name and port without getting an instance of the adapter.
 
  System.out.println("Default Adapter: " +
                      OneWireAccessProvider.getProperty("onewire.adapter.default"));
  System.out.println("Default Port: " +
                      OneWireAccessProvider.getProperty("onewire.port.default"));
  

Version:
0.00, 30 August 2000
See Also:
DSPortAdapter

Method Summary
static Enumeration enumerateAllAdapters()
          Gets an Enumeration of all 1-Wire adapter types supported.
static DSPortAdapter getAdapter(String adapterName, String portName)
          Finds, opens, and verifies the specified adapter on the indicated port.
static DSPortAdapter getDefaultAdapter()
          Finds, opens, and verifies the default adapter and port.
static String getProperty(String propName)
          Gets the specfied onewire property.
 
Methods inherited from class java.lang.Object
equals, getClass, hashCode, notify, notifyAll, toString, wait, wait, wait
 

Method Detail

enumerateAllAdapters

public static Enumeration enumerateAllAdapters()
Gets an Enumeration of all 1-Wire adapter types supported. Using this enumeration with the port enumeration for each adapter, a search can be done to find all available hardware adapters.
Returns:
Enumeration of DSPortAdapters in the system

getAdapter

public static DSPortAdapter getAdapter(String adapterName,
                                       String portName)
                                throws OneWireIOException,
                                       OneWireException
Finds, opens, and verifies the specified adapter on the indicated port.
Parameters:
adapterName - string name of the adapter (match to result of call to getAdapterName() method in DSPortAdapter)
portName - string name of the port used in the method selectPort() in DSPortAdapter
Returns:
DSPortAdapter if adapter present
Throws:
OneWireIOException - when communcation with the adapter fails
OneWireException - when the port or adapter not present

getDefaultAdapter

public static DSPortAdapter getDefaultAdapter()
                                       throws OneWireIOException,
                                              OneWireException
Finds, opens, and verifies the default adapter and port. Looks for the default adapter/port in the following locations:

Returns:
DSPortAdapter if default adapter present
Throws:
OneWireIOException - when communcation with the adapter fails
OneWireException - when the port or adapter not present

getProperty

public static String getProperty(String propName)
Gets the specfied onewire property. Looks for the property in the following locations:

Parameters:
propName - string name of the property to read
Returns:
String representing the property value or null if it could not be found (onewire.adapter.default and onewire.port.default may return a 'smart' default even if property not present)